Hello,
i'm using MSP-TS430PM64 evaluation board and try to configure TIMER0 clock source
When i use SMCLK as source code i get interuption but if i want to use ACLK (32768 Hz) i get no interruption.
I just replace in my code :
//SMCLK used devided 1MHZ by 8 = 125KHz
TACTL = TACLR | MC_0 | ID_3 | TASSEL_2;
by
//source is selected as ACLK (32768 Hz)
TACTL = TACLR | MC_0 | ID_0 | TASSEL_1 ;
then timer 0 complete initialization is :
CCTL0 = CCIE; // CCR0 interrupt enabled
//time based on 250ms
CCR0 = TIMER_BASE_250MS;
//start timer mode continuous : MC_2
TACTL |= MC_2;
Do you know why i get no interuption ?
Thanks