Other Parts Discussed in Thread: ENERGYTRACE
Tool/software:
Hi Experts,
I'm working on a project using the MSP430FR5994, and I'm aiming to drive an LED with the lowest possible power consumption. Currently, I'm driving the LED by toggling a GPIO pin, and it works fine with higher clock frequencies. However, when I reduce the master clock frequency to 32 kHz (ACLK), the LED fails to light up.
My goal is to use the lowest possible clock frequency to drive the LED while minimizing power consumption. Could you please advise on the following:
- What is the minimum clock frequency required to effectively drive an LED using GPIO pin toggling?
- Are there any alternative low-power methods for driving an LED with MSP430FR5994, possibly using PWM or another approach, that would work at lower frequencies like 32 kHz?
I appreciate any suggestions or guidance you can provide.
Thank you!
Regards,
Josel