Dear All,
Could you please help us to understand following errata statement clearly.
Referring to the document "MSP430F47x Device Erratasheet",
Does the statement
"When a flash write or erase is abruptly terminated, any further reliable reads by the flash
controller are not ensured. The abrupt termination can be the result of one the following
events:" means that the flash is dead any more or is the flush not functional temporarirly and if yes when will the normal operation of flash restore?
The reason why we are asking is the abrupt termination of the flash could also occur in the case of a power failure and under a strong EMI exposure which are unavoidable most of the time.
Regards,