This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-GANG: ERROR 308: Communication Port baud rate change

Part Number: MSP-GANG

Tool/software:

Hello,

I have downloaded the MSP-GANG Software, installed all drivers, and connected my production programmer to my PC. It recognizes that the device is connected to the computer at COM3, but when I open the software it rapidly cycles through and repeats these messages:

ERROR 308: Communication Port baud rate change (x4)

Changing Baudrate...

Changing Baudrate... Failed

I have tried installing/ uninstalling the software and drivers several times now. Restarting computer etc. The software is completely locked up with this.

On the programmer itself, the LCD just says, "Image 1.0(Err!)". If I click the arrow, the number cycles from 1.0-10.0 then lands back at 1.0. 

I don't have the power cable and I am 90% convinced I have the correct MCU information. Could either or both of these be my issue? If I do have the wrong MCU information, how do I find the right information?

**Attention** This is a public forum