Hello,
I have been developing a system for controlling DC motors based on MSP430F2254 for the past two months and everything work without problems. I decided to add a simple RS-232 monitor that can be activated with sending a character from PC. The function of the RS-232 is that the user can manually control the motor by enering command to the hyperterminal of the PC. I initialized the USCI, wrote my code and programmed the MSP430F2254 and it works as expected. But when I remove the FET430UIF programmer from the Jtag controller of my PCB the microcontroller starts acting very bizzare. The RS 232 communication fails, the DC motors starts moving randomly. I do a POR but there is no effect.
If anyone has encounter a problem of this sorts with the FET430UIF I'll appreciate the help
Thank you