This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am trying to read from A3 and A4 inputs to the processor. I can read A3 fine, but when I try and read A4, I get the same value. With the debugger I can see that I am correctly changing ADC12MCTL0 depending on which parameter I call the function with, so I am assuming there is something else wrong with how I am reading the result registers? Any help would be greatly appreciated.
uint16_t adcResult = 0x0000; void initADC(){ while(REFCTL0 & REFGENBUSY); // If ref generator busy, WAIT REFCTL0 |= REFVSEL_2 | REFON; // Select internal ref = 2.5V ADC12CTL0 = ADC12SHT0_2 | ADC12ON; ADC12CTL1 = ADC12SHP; // ADCCLK = MODOSC; sampling timer ADC12CTL2 |= ADC12RES_2; // 12-bit conversion results } uint16_t sampleADC(ADC_Input channel){ //select right channels from the ADC switch(channel){ case ADC_CH_REG_3V3: ADC12MCTL0 = ADC12INCH_4 | ADC12VRSEL_1; // A1 ADC input select; Vref=+VRef break; case ADC_CH_INA241: ADC12MCTL0 = ADC12INCH_3 | ADC12VRSEL_1; break; } while(!(REFCTL0 & REFGENRDY)); //make sure reference has settled ADC12IER0 |= ADC12IE0; // Enable ADC conv complete interrupt ADC12CTL0 |= ADC12ENC | ADC12SC; // Enable and start sampling/conversion __bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupts return adcResult; } //********************************************************************************************** //** ADC Interrupt routine ********************************************************************* //** Called when the corresponding ADC12MEMx memory register is loaded with a conversion result //********************************************************************************************** #pragma vector = ADC12_B_VECTOR __interrupt void ADC12_ISR(void) { switch(__even_in_range(ADC12IV, ADC12IV__ADC12RDYIFG)) { case ADC12IV__ADC12IFG0: // Vector 12: ADC12MEM0 Interrupt adcResult = ADC12MEM0; // Exit from LPM0 and continue executing main __bic_SR_register_on_exit(LPM0_bits); break; } }
Thanks Bruce, an easy fix. That's actually quite clear in the user guide, not sure how I missed it. Appreciate the help.
**Attention** This is a public forum