Part Number: MSP-EXP430G2ET
Other Parts Discussed in Thread: TCA6424A, MSP430G2553, IO-EXPANDER-EVM
Tool/software:
Hello,
I have the MSP-EXP430G2ET EVM (with the MSP430G2553 populated) and the IO-EXPANDER-EVM. I've been following the instructions on the IO-EXPANDER-EVM User Guide (SLVUA59A) to test the TCA6424A.
When I run the IO Expander Flash.bat, I get the following cmd window:
Programing IO_Expander.txt into MSP430G2553 ......
* -----/|-------------------------------------------------------------------- *
* / |__ *
* /_ / MSP430 Flasher v1.3.0 *
* | / *
* -----|/-------------------------------------------------------------------- *
* Evaluating triggers...done
* Checking for available FET debuggers:
* Couldn't find any connected USB FETs!
# Exit: 11
# MSP DebugStack not initialized
* Starting target code execution...done
* Disconnecting from device...done
*
* ----------------------------------------------------------------------------
* Driver : closed (MSP DebugStack not initialized)
* ----------------------------------------------------------------------------
*/
--------------------------------------------------------------------------------------------
When I check the COM ports, all I see is this:
and I don't see the "MSP430 Application UART" port as shown in the IO Expander EVM User Guide.
I've tried running the files as administrator and that didn't work.
I installed CCS but the MSP-EXP430G2ET is not listed in CCS.
Please advice on what to do to get the microcontroller working.
Let me know if further information is needed.
Thanks