This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430I2041: SD24 single end input voltage range that can mesure.

Genius 3066 points
Part Number: MSP430I2041

Tool/software:

Hello.

I believe MSP430I2041's SD24 can use as single end input (A+ is input, A - connect to GND)

I believe it allowd input -1 (AVss=0V) to Vcc.

in this situation, Is the A+ can mesure up to -928 to +928mV? or minimum is AVSS?

And if A- connect to +1.5V, is A+ can mesure +572 to 2428mV? or up to Vref?

I want to confirm is the A+ can mesure if input was over reference voltage.

Best Regards,

GR

**Attention** This is a public forum