Tool/software:
Hello,
I am a little bit confused with the USCI UART. Despite, many times I successfully used the old UART module in F1xxx, F4xx family.
Using USCI, I get much lower baud rate that I except. My SMCLK clock is: 46*32768Hz.
My UART config:
BIS.B #081H,&UCA0CTL1 ;SMCLK source + RESET port
;BIS.B #000H,&UCA0CTL0 ;8bit, 1stop, LSB first
MOV.B #79,&UCA0BR0 ;lower byte Baud rate: 19200 , 1,50732MHz/19200=79
MOV.B #0,&UCA0BR1 ;upper byte
BIS.B #11110001B,&UCA0MCTL ;UCOS16 set->needed for high frequency clock, Oversampling, BRFx=15
BIS.B #1,&IE2 ;RX IE, IFG2 register to reach FLAG
BIC.B #1,&UCA0CTL1 ;remove reset
Bit time is about 1.1ms measured by scope ! I tried with 'UCOS16' bit =0 much close to desired but with BR0=89 value.
Can somebody give some advise where can be the problem?
Thanks and regards,
Joseph