Part Number: MSP430F6779
Tool/software:
Hi Team,
1. With what sampling rate the 24-bit ADCs are working in this MCU?
2. UP tp what harmonic this MCU can calculate accoridngly?
Regards,
Maryam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F6779
Tool/software:
Hi Team,
1. With what sampling rate the 24-bit ADCs are working in this MCU?
2. UP tp what harmonic this MCU can calculate accoridngly?
Regards,
Maryam
Hi,
The fsd = 2.3MHz max. The OSR is from 1 to 2048. So, the sampling rate would be 2.3M/24bit/1 to 2.3M/24bit/1024, which is from 95.8k to 93.58Hz
Use 95.8kHz sampling rate for example. 95.8k/10/2 = 4.79k, 4.79k/50Hz = 95th. It can calculate harmonics up to the 95th harmonic of a 50Hz frequency.
Best regards,
Cash Hao
**Attention** This is a public forum