1. I am working with msp430f235 And it is being programmed using msp430FETUIF. May I know that apart from 48 general input and output pins, how rest of the pins should be connected in order to burn a program in msp430?
2. As 48 pins are general input- output. Is there any pin, which is mandatory to connect, while its operation OR all 48 pin are optional to use?
3. If I am using internal reference for ADC12. So where should I connect external voltage reference pins?
4. On the Target board VCC & GND pins are provided separately. So Should I also connect pin 64 & 1 to Vcc ?
5. May I get any learning material related to "connections of pins of msp430f235" from Texas Instruments's side ?