Part Number: MSP430F67791
Other Parts Discussed in Thread: MSP-EXP430F5529LP, MSP-FET
Hi TI team!
I am following the steps specified in the link file:///C:/ti/msp/EnergyMeasurementDesignCenter_1.40.00.03/EnergyMeasurementDesignCenter/docs/users_guide/html/Energy_Measurement_Technology_Guide_html/markdown/ch_designcenter.html#introduction to connect the EVM430-F6779 board using high voltage (i.e., with direct external power from the mains) and be able to view the data on the computer, thus having:
1. The MSP-EXP430F5529LP launchpad flashed with the base code shown in the guide.
2. The EVM430-F6779 board flashed via the MSP-FET with the base code shown in the guide.
3. The connection between the EVM, the launchpad, and the Isolation Plugin Board.
The final step is to connect to the Launchpad and open the results section in the Energy Measurement Design Center program. However, when connecting, I get the error: "HID device connected, but could not connect to it."
I tried to solve the problem by connecting everything to another computer, but I got the same error. I don't know what else I can do.