I am working with msp430 f235. the input signal that is given to ADC12 of msp430 is 150mV sin signal.The negative input voltage range that msp430 can sustain is -0.3V. Would such a input signal can affect the performance of ADC12 ? because the negative reference given to ADC12 of msp430 is 0V.