Hi,
I am trying to design up a system that will use the MSP430F5507 in production and would like to blow the fuse to protect the code. Is it possible to blow the fuse through a USB connection? I am assuming no.
Second, what if I design the setup with the D+ and D- lines of the USB connected to the RST and TEST pins, in parallel, for programming one time and blowing the fuse. I would of course use a modified USB connector and the FET programmer. After the fuse is blown I would use the USB D+ and D- lines as specified for USB communication, but the RST and TEST lines for Spy-Bi programming would still be physically connect to the D+ and D- lines. Would this cause problems when using in USB mode and sending signals to RST and TEST pins on the msp430, or is it that once the fuse has been blown these lines no longer affect the MSP430?
Thanks,