I'm usinf CCS5.1 to develop code for an MSP430F4616. Since I'm familiar with the StellarisWare package, I was hoping to use the MSP430Ware driver library. However, I see things like MSP430Ware supports "ALL MSP430 devices" followed by the statement that "MSP430 Driver Library supports 5 and 6 series devices." Which is correct?
Is there a way to use the MSP430 driver library for the MSP430F4616? AT first glance it looksas though I should be OK, but I don't want to be barking up the wring tree!
What lead me to the E2E forum is the question: For the MSP430F4616 where is something like __MSP430_BASEADDRESS_PORT1_R__ defined?
Thanks