Customer question on a MSP430G2213 detail -
I'm using the comparator with the output going to P1.3/CAOUT to trigger some external hardware. I also want to time the comparator. I see the timer output connects to Timer_A CCI1B, correct? If I set up Timer1_A3 CCR1 to capture edges on CCI1B it looks like the comparator output will also appear on that pin (p2.2) - is that correct? I thought I could connect the comparator output direct to the timer without a pin, but maybe not?
Thank you !
Mike