what kind of decoupling capacitor should be used for Msp430g2101. Please send me complete specification of it
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
what kind of decoupling capacitor should be used for Msp430g2101. Please send me complete specification of it
http://dangerousprototypes.com/docs/MSP430_quick_start
and
http://www.diylife.com/2008/03/28/program-a-msp430-microcontroller-pt-2/
both agree in 0.1 uF
Being ignorant (or lucky), I have used can-type polarized 16 V 47 uF just fine - YMMV.
dangerous prototypes says:
"Put a 0.1uF decoupling capacitor on each positive supply pin, and put it as close to the chip on your PCB as possible"
**Attention** This is a public forum