I compiled and ran the USBCDC_Example1 and was able to turn on / off and toggle slow and fast the LED.
However I need help on the following 2 problems:
1. The compiler generates the following warning: I am using the Code Composer Studio Core Edition Version: 4.0.2.01003T
"This project was created using a version of Code Generation tools that is not currently installed: 3.1.0 [MSP430]. Please install the Code Generation tools of this version, or migrate the project to one of the supported versions. "
How to get rid of this warning?
2. I used MSP-TS430PN80USB kit and MSP-FET430UIF to download and run the program. When I disconnect the MSP-FET430UIF from the Laptop the board stops working. I thought the program is running in the Flash and I do not need the MSO-FET430UIF.
How do I run this program stand alone by the USB Kit without the USB debugging interface?
Thanks.