Hi,
I am using MSP430F2419 device which is having ADC12. I using the internal reference voltage(2.5V) and as per the design I have provided two external capacitor 10uF/10V and 0.1uF/10V across VRef+ and VRef-. Iam doing the following configuration in my code to enable internal reference, but I could able to get either 2.5V or 1.5V in the VRef+ Pin outs.
Also for ADC10 we have a REFOUT bit, but it is not in ADC12. How can I ensure, that my internal voltage is set perfectly without measuring it on the VRef+ pin out?
ADC12CTL0 = ADC12ON+REFON+REF2_5V+SHT0_8+MSC;
ADC12CTL1 = SHP; // Use sampling timer,
ADC12MCTL0 = INCH_2+SREF_1; // ref+=AVcc,AVss channel = A2
ADC12MCTL1 = INCH_3+SREF_1; // ref+=AVcc,AVss channel = A3
ADC12IE = INCH_2+INCH_3;
Thanks in Advance,
Regards,
V.Yuvaraj