Hi,
Is there any changes required in my SPI code , it is in four pin mode with external GPIO pin as chip select(so 3-pin)
i am using msp430f1481, problem is that with bitbanking method i was able to transmit data and receive with an external flash,but with
inbuilt SPI some times it is and some times it is not, why actually happens this?Am i left any thing in SPI initialization?
below is my SPI initialization
SPICLK is 1 MHz
void SPI_Enable(void)
{
unsigned volatile i;
P5SEL |= 0x0E; // P5.1,2,3 SPI option select
P5DIR |= 0x0A;
P4DIR |= 0x08; //External pin as chipselect
P4OUT &=~0x08; //Reset Slave
U1CTL = CHAR + SYNC + MM + SWRST; // 8-bit, SPI, Master
U1TCTL = SSEL1 + STC; // Mode 0, SMCLK, 3-wire
U1BR0 = 0x02; // SPICLK = SMCLK/2
U1BR1 = 0x00;
U1MCTL = 0x00;
ME2 |= USPIE1; // Module enable
U1CTL &= ~SWRST; // SPI enable
for (i = 0xFFF; i > 0; i--); // Time for slave to ready
_BIS_SR(GIE); // Global interrupt
}
Thanks & Regards
Kshatriya