Hello!
I'm beginner in using MSP microcontrollers and now I have a question about flashing MSPF2132 with ez430-rf2500 tool.
MSP430F2131 support 2-wire jtag programming, also ez430-rf2500 support that type onMSP430F20/21/22 series. I got microcontroller MSP430F2132 and I just can't debug program code from CCE v3.1. Pins Vss, Vcc, RST and TEST are connected in right place, but when I want to debug my project, pop-up window say that: "Error connecting to the target:No MSP430 device was found on USB FET 1".
In project propertis I select "Device variant" and "Linker Command File" to F2132.
Has anybody know what I'm doing wrong?