Hello,
I'm trying to develop a system to transmit information wirelessly from the MSP-EXP430FG4618 experimenters board to a PC.
I'm thinking of ordering the "CC2500EMK Evaluation Module 2.4 GHz" so as to be able to add an antenna and transceiver to the experimenters board.
Would it be possible to connect the other antenna and transceiver circuit which comes with the evaluation module directly to the PC, and communicate this way between the two?
Also, I was thinking of using the MSP-EXP430FG4618 experimenters board as an end-point in a network with the access-point being an EZ430-RF2500 connected to the PC, and communicating between the two using SimpliciTI. Would this be feasible?
Thanks for any help.
Mike