Hello:
I have designed the CC430F6135 into a new project that is battery operated. I would like to use the on-chip RTC to save some space/cost on my project. We need to keep the RTC going when the unit is unpowered so that the time/date remain correct. I have a CR2032 battery on the board to power the CC430F6135's RTC during those times when the system is shut down, but I'm not sure which power pin(s) to drive with the battery. Do you have any suggestions on how to keep the RTC alive from the battery without having all the other loads on that would draw extra uA?
Any feedback or input is welcomed and appreciated!
Thanks again!
Paul