Hello:
I would like an MSP430FR5729 to talk to an MSP430F2232 over RS-485 at a baud rate faster than 9600, but I was planning on using a 32kHz crystal on both in order to go into LPM3. Some MSP430s have an XT2 connection for two crystal inputs, but I don’t think these have that option. Is the DCO accurate enough over temperature (-40C to+85C) to support a UART? If not, what are my options for supporting LPM3 and a UART? Accuracy of the clock for waking up from LPM3 is important.
Thank you for your help! Any feedback or input is welcomed and appreciated!
Best regards,
Paul