Hello,
I am attempting to connect a CC2520 to an MSP430F5521 via SPI, but have no idea where to begin.
Any pointers to the right direction would be greatly appreciated.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am attempting to connect a CC2520 to an MSP430F5521 via SPI, but have no idea where to begin.
Any pointers to the right direction would be greatly appreciated.
Hi,
are you planning to use zigbee? I would recommend to take a look at the ZAP Implementation using MSP430F5438A on MSP-EXP430F5438 (http://www.ti.com/tool/msp-exp430f5438) and CC2520 on CC2520EMK (http://www.ti.com/tool/cc2520emk - http://www.ti.com/tool/CC2520EM_REFDES)
Hope this helps.
I am just currently attempting to do a simple 'hello world' packet broadcast via 802.15.4, and nothing as complicated as a network protocol. Are there any code examples of sending instructions from the MSP to the CC2520 (such as initializing and tx)? If the previous reply had an example, I could not locate it.
Hi Tim,
you can either download the example code here: http://www.ti.com/litv/zip/swrc090b or take a look at SimpliciTI protocol stack: http://www.ti.com/tool/simpliciti besides of course the z-stack: http://www.ti.com/tool/z-stack
Hope this helps.
I am currently using the example code, but have modified the assy_ccmsp2618_cc2520em.c and .h interfacing code to work with the MSP430F5521.
Now I have received an 'unresolved symbols remain' error.
Currently the console outputs a number of undefined symbols (such as BCSCTL1) and where it was first referenced in file (such as ./components/targets/srf05_ccmsp2618/hal_mcu.obj ).
undefined first referenced symbol in file --------- ---------------- BCSCTL1 ./components/targets/srf05_ccmsp2618/hal_mcu.obj CALBC1_1MHZ ./components/targets/srf05_ccmsp2618/hal_mcu.obj CALDCO_1MHZ ./components/targets/srf05_ccmsp2618/hal_mcu.obj DCOCTL ./components/targets/srf05_ccmsp2618/hal_mcu.obj IE2 ./components/targets/srf05_ccmsp2618/hal_uart.obj P1DIR ./components/radios/cc2520/hal_rf.obj P1IE ./components/targets/srf05_ccmsp2618/hal_digio.obj P1IES ./components/targets/srf05_ccmsp2618/hal_digio.obj P1IFG ./components/targets/srf05_ccmsp2618/hal_digio.obj P1IN ./components/radios/cc2520/hal_rf.obj P1OUT ./components/radios/cc2520/hal_rf.obj P1SEL ./components/targets/srf05_ccmsp2618/hal_digio.obj P2DIR ./components/targets/srf05_ccmsp2618/hal_uart.obj P2IE ./components/targets/srf05_ccmsp2618/hal_digio.obj P2IES ./components/targets/srf05_ccmsp2618/hal_digio.obj P2IFG ./components/targets/srf05_ccmsp2618/hal_digio.obj P2OUT ./components/targets/srf05_ccmsp2618/hal_uart.obj P2SEL ./components/targets/srf05_ccmsp2618/hal_uart.obj P3DIR ./components/targets/srf05_ccmsp2618/hal_digio.obj P3OUT ./components/targets/srf05_ccmsp2618/hal_digio.obj P3SEL ./components/targets/srf05_ccmsp2618/hal_uart.obj P4DIR ./components/targets/srf05_ccmsp2618/hal_joystick.obj P4OUT ./components/targets/srf05_ccmsp2618/hal_led.obj P4SEL ./components/targets/srf05_ccmsp2618/hal_joystick.obj P5DIR ./components/radios/cc2520/hal_rf.obj P5IN ./components/radios/cc2520/hal_rf.obj P5OUT ./components/radios/cc2520/hal_rf.obj P5SEL ./components/targets/srf05_ccmsp2618/hal_digio.obj P6DIR ./components/targets/srf05_ccmsp2618/hal_lcd.obj P6OUT ./components/targets/srf05_ccmsp2618/hal_lcd.obj P6SEL ./components/targets/srf05_ccmsp2618/hal_joystick.obj P7DIR ./components/targets/srf05_ccmsp2618/hal_digio.obj P7OUT ./components/targets/srf05_ccmsp2618/hal_digio.obj P7SEL ./components/targets/srf05_ccmsp2618/hal_digio.obj P8DIR ./components/targets/srf05_ccmsp2618/hal_digio.obj P8OUT ./components/targets/srf05_ccmsp2618/hal_digio.obj P8SEL ./components/targets/srf05_ccmsp2618/hal_digio.obj UC1IFG ./components/radios/cc2520/hal_cc2520.obj error #10234-D: unresolved symbols remain
Hii Tim Lam,
I am doing a project on 'implementation of zigbee communication module'. I am ready with my hardware part . Now , I want to work my cc2520 using msp430 microcontroller. I want to send instructions to initialise cc2520,for setting its mode.Before proceeding further I just want to transmit "hello" and display it on LCD on receiver side.But I have no idea from where to start.I am completely new to this thing.Can you please help me out ?? Can you tell me how to use Z-stack for this puspose??
**Attention** This is a public forum