I am using a MSP430F4784 making a/d samples on each of the 4 channels. I have the inputs connected to a bench precision voltage source. I am receiving very stable A to D data with a consistent reading. Leaving everything the same except cycling power on the MSP430, I once again receive a stable signal but 6-8 counts plus or minus than the original each time the power is cycled. This error occurs in all channels and are offset by about the same amount.This leaves me to believe that the problem is in the common circuitry inside the A to D.
Is there something I need to do to correct this situation?
Thanks for the help,