Hi. Long time lurker. First time poster..
I recently acquired a reel of 30 MSP430FR5728 chips (QFP). Haven't been able to put them in to BSL mode using my Launchpad- the MSP430FR5728 runs user code (main) instead of the BSL code. Does anybody know if these chips ship with a BSL? I've been using the following pins to try and put the MSP430FR5728 in to BSL mode with no success: RST, TEST, 2.0 (TX), 2,1(RX). Am I using the correct pins? The BSL specification defines two BSL entry sequences and I have been trying both. Should I be using one over the other?
Thank you for your help!!