Hi,
430AFE223 has two SD24 converters and each converter has only one analog signal pair with it. I believe this since in the CPU i/o pin configuration in the datasheet, it shows the 3 pair signal pins for this ADC inputs.
On the other hand, from the fig 27.1 in slau144i.pdf, it shows each channel of the ADC has the Eight input pair. If this is true, the CPU i/o pin should show 16 pair i/o signals on the i/o pin configuration.
Please confirm that the datasheet is correct and(fig 27.1 in slau144i.pdf is not correct) or...
Thanks,
Mark