To all concerned:
I'm working a project requiring a large ZigBee mesh network, of which each node requires a delta-sigma ADC (minimum 16-bit) to do its task. I've been able to rough out the ADC interface using a MSP430F2013 and a LaunchPad, but there's not nearly enough memory for a Z-stack. My thought is to use a MSP430AFE251, as it includes an SD24 and lots of memory, paired with a CC2520 for the wireless. (Part cost is key, so while I could pair the '2530 with an ADC, the cost is greater than the '251/'2520 solution.) The next step in my development is to rough out the network stuff, to include using signal strength as a way to let the network physically self-actualize node locations (relative to one another). I'm trying to minimize the outlay of cash, and am weighing two options. One, use the CC2530 development modules to rough out the network stuff, and assume the '251 will handle the rest. Two, use the CC2520 development modules, but wire them to a 24-pin socket target board with the '251, and thus effectively prototype the end product. The former is relatively inexpensive for a two node kit, but the latter could get pricey, especially as it needs a programmer to go with the target board. Therefore, I suppose I have two questions:
1) Does the '251 have enough memory to run the Z-stack when paired with a '2520? I've read through a lot of documentation, and "required memory" doesn't seem to come up in the discussion.
2) Any recommendations on cost-effective prototyping, assuming the answer to #1 is yes? Method A, B or a better alternative?
Thanks in advance for any guidance anyone can offer.
--Ken