I am planing to use the internal Vref of the MSP430G2513 amongst others for a temperature measurement. According to the datasheet Vref 1,5V has a tolerance of +/-0,9V. So does this mean, that for one chip the Vref varies within the limits over the time, or is it for one chip one fix value between the limits? Supposed it is a fixed value, a one point calibration for the temperaturemeasurement would eliminate the error of the reference voltage and a user-calibration for the reference voltage by measuring Vref on a output pin would be possible?