Hi,
I am using MSP430AFE232 for one of my applilcation where I will be measuring load current using CT. This controller has two 24-bit Delta Sigma ADCs. Could you please help me in converting the ADC output raw data to real data using some formula. I have been trying with standard equation that uses reference voltage and number of bits, but not getting the correct data. And also if I use both of the two channels then the controller is getting damaged. The maximum voltage that will be applied to each of the channel is 150 mV (AC).