Hi,
Im using the Grace code generator to configure my MSP430G2432. I dont quite understand the note that "configuring the flash controller is only needed in case of using in-system application self-programming techniques". In my application, the MCU communicates via SPI with two slave devices and needs to process incoming analog signals. Should I enable the flash controller?
Concerning the ADC, Grace offers the possibility to eable 2'Complement and Automatic Data Transfer Controller. When do I need these functions?
Thanks a lot!
Best regards