Good afternoon, The consultation relates to a problem with the useful deduggear "MSP-FET430UIF" microcontroller "MSP430FR5724" The environment used is the "Code Composer Studio Version: 5.1.1.00031" and the leading compiler of Texas. If you use the IAR environment the same problem occurs.
1) With a microcontroller PCB that has the "MSP430FW425" is everything OK.
2) Using a microcontroller PCB that has the "MSP430FR5724" proffers no deduggear, gives the error:
Error connecting to the target: Unknown device
PCBs are similar using the same pin JTAG. - PJ.0 / TD0 - PJ.1 / TDI - PJ.2 / TMS - PJ.3 / TCK - RST / NMI
NOTE: The firmware of "MSP-FET430UIF" is updated. I would like to know what can be the problem or attack???
regards, Jose Miguel