Hello everybody,
I have got some questions about the current consumption of the 16bit ADC of the MSP430F2003. Lets say I want to work with 1MHz at 3V and a gain of 1 is enough. In this case the Datasheet tells me, that the current consumption of the ADC-module is 730µA (SD16LP = 0).
1) does the TemperatureSensor take additional current?
2) does every channel take this 730µA?
3) is there a possibility to turn channels selectively off (in order to save power)?
4) are those 730µA maximum ratings or may the ADC even take more current in special settings?
I did not found any information regarding my questions in the Datasheet or UsersGuide.
Thanks in advance. Regards.
Ben