I have a couple of questions regarding programming the CC430F5135:
1. When using the MSP430 Flasher command line utility and the MSP-FET430UIF I get the error:
Accessing Device...
Exit: 16
ERROR: Unknown Device
I believe the device is connected and powered properly. I can use Elpotronic's FET-Pro430 programming tool, and it works fine. The programmer also works fine when using it as a debugging through Code Composer Studio. This error only occurs when using the command line utility. I'm using the Spy-Bi-Wire interface. I have the latest version of MSP430 Flasher (v1.2.1). I've tried several versions of FW on the MSP-FET430UIF, and none of them work.
2. How long should it take to erase, program, and verify a 16K CC430? It currently takes around 30 seconds using the Elpotronic tool with MSP-FET430UIF. Is the GANG programmer faster? Is the 4-wire interface significantly faster than the 2-wire interface? Are there any other options that will program faster?
Thanks,
Chad C.