Hello E2E,
My goal is to jump into the BSL code from an embedded function call. This would allow the firmware image to be updated via the serial port. I have read that certain chips have a customizable BSL area, but the MSP430F4XX has a fixed unchangeable area. My plan is to use the fixed ROM BSL program to reprogram the images without the need of using external signals to enter BSL mode.
What address or how would I jump to the BSL program using a jump instruction or function call? Is this possible? This is for the MSP430F477.
Thanks,
Andrew Perkins