I would like to know what are the external component requirements of the reset circuit on a MSP430BT5190 micro controller. From what I have read, there seems to be some confusion.
I intend to run the micro off a CR coin cell battery (2.0 to 3.2V), with standard 6 wire programming, and (if possible) would like to use components that are already used on the board (10k, 100k, 100nF, 1uF). The standard values seem to be a 47k pull up, with a 2.2 nF pull down, however 10k pull up and 100 nF pull down is also mentioned. Then, some threads refer to later series MSP models having resistors or capacitors inside the chip.
Does the MSP430BT5190 have any pull ups / downs within the chip, and what range of components would work for my circuit?