This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error initializing emulator: The voltage 1162 value is not correct/allowed for the USB FET

Other Parts Discussed in Thread: MSP-TS430PN80

Hi all,

Just looking for help with my CCS -> FET.  The details of my installation are:

  • Fresh, clean installation
  • version 5.4.0.00091
  • Host is Ubuntu 13.04 laptop.  Linux command 'lsusb' shows the FET tool as I expect to see it
  • Connected to MSP FET 430 UIF (firmware version 3.03 I think)
  • FET tool is connected to a MSP-TS430PN80 USB target board
  • Target board is populated with a 430F5529 chip
I double click on the first MSP430F552x One-Click Project File in the 'resource explorer' - flash the damned LED - and a simple project is created for me.  I click to debug, code compiles fine and then I get the error:
    Error initializing emulator: The voltage 1162 value is not correct/allowed for the USB FET
Sometimes the 1162 is a different but similar number.  The project Target Configuration -> Target -> Target Voltage is still at the default 3000.
I can't be the first to have this problem, but I can't find anything like this using Google.
Any ideas?
Thanks!
  • Sorry everybody - Chester has pointed out my rookie mistake.  so embarrassed as I don't really think of myself as a rookie...  Wrong power supply jumper setting - I've been looking for the complicated problem rather than the obvious.

**Attention** This is a public forum