Our customer's applications have boards some using the MSP430F5438A and some using the MSP430BT5190. They are adding a function to the test programs to identify which microprocessor is installed on the boards. It is simple enough to read the Device Descriptor table to determine the device ID and hardware revision.
However, it look like both of these processors are using the same Device ID (0x05,0x80). Is there another chip ID that can be read to determine which of these chips is in use?