I want to use SVS functionality with the MSP430F250. But I was surprised that I did not found a definition for the register SVSCTL. I looked for other registers used in the program and they are declared with a macro, which is:
#define SFR_8BIT(address) extern volatile unsigned char address
I do not know how to specify the address if I declare SFR_8BIT(SVSCTL);
I want a Voltage level detect of 2.3V with PORON reset, so the code was supposed to be:
SVSCTL = 0x48;
How do I solve this? Is the control register for SVS called different?