Hello together,
I have a problem which I want to solve with your help:
I have application with the MSP430F2002 which is programmed with the TI GANG430 programmer.
I can program, verify and blow the fuse with the GANG430.
But after programming , I have a test station to verify the function of the complete application and if all test are passed, I want to blow the fuse without a jtag programmer.
My actual process isto power the device and apply 6,5 V to the TEST pin and after 2 ms I rised the RESET pin for 1 ms to start the blow mechanism, but nothing happens. Its not possible to add a jtag programmer to this station, so I must do it in the simple way.
Can you please help to to find a process to blow this fuse
Best Regards,
Michael