Board Info: EM430F6137RF900 Rev. 3.2 EB1
I'm using Code Composer to load the following example onto the boards: slac525a\SLAA465 - CC430 RFExamples\CC430x613x\RF examples\ ExamplesCC430x613x RF examples\Asynchronous_Communication
I load one with RX and one with TX using 915 Mhz. (I've also tried 868Mhz)
I'm expecting the green LED on the RX board to only light up once it receives the signal from the TX board. However, the second I load the RX board, the green LED turns on even when the TX board is off.
Any idea what might be going wrong?
Thanks for the help in advance.