Hi,
In the datasheet of MSP430F147 says that:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In the datasheet of MSP430F147 says that:
No. Because the creator of this current calculator apparently failed to perform simple math for checking his code.David V said:Is that correct?
Enter 10mAh capacity and 1mA load, you won't get 10hrs but 7 instead. At first, I suspected some clever consideration of self-discharge for long discharge times, or capacity vs. load (load rating) compensation, but no. The result is always off by a factor of 0.7, no matter if you discharge the battery in 1 hour or 1000 hrs, with high or low current.
So with 1Ah battery and 280µA current consumption of the MSP, the battery should last for 3571hrs = 149 days (minus self-discharge)
But this means the MSP is not doing anything. Not using RS232, not doing A/D conversion, not driving any digital circuity or sensing buttons. These 280µA are the plain CPU/memory consumptions. Including the specified clock source for the CPU.
Note, that battery capacity is rated for a certain load. So a battery that has a capacitance of 1Ah for a load of 1A will be able to provide, say, 1.2Ah if the load is 100mA only. But due to self-discharge, the effective capacity will drop to 0.9Ah when the load is only 1mA.
Usually, the manufacturer picks the condition that gives the highest effective capacity. Looks better in the datasheet.
Hi Jens,
Thanks for the answer.
Ok when I say MY uC will use UART then the consumption will go up. Is there a way to predict the consumption or I have to connect an AMP meter to determine the consumption?
Regards.
**Attention** This is a public forum