Hi Friends,
I have a small question and the case is as below.
I have MSP430F2012 with EZ430-T2012 Board
I have 2 motors connected through a motor driver which accepts pwm/dir input.
I have a joystick with 2 analog outputs.
and my progress so far.
- I am using grace to config
-I can read the ADC for the joystick values and processed them for pwm values and direction for gpio.
-TimerA has 2 channels I have selected P1.5(TA0), P1.6(TA1) for outputs
- in grace i have set both block 0 and 1 in PWM mode.
what I need to know
In the grace i see duty cycle for only block 1 and not for block 0
how do I Config the PWM for the motors from these 2 channels ?