I am using MSP430F4793 analog input 0
I find that when conversion is started some noise is generated. I assume this is because the SD16 is being powered up whenever a conversion is started in single coversion mode.
I am running a single conversion each 250mS.
When I run the ADC in continuous mode, I don't see this noise. However its a battery powered application and I can't run the ADC in Continuous mode.
The ADC input is being driven by an OpAmp as a preamplifier. I I install 10K resistors between the output of the opamp and the ADC input the startup noise is reduced by a quarter, but this is not the best solution and doesn't eliminate the noise. I have tried using the internal reference instead of an external reference, but to improvement occured.
It appears as a decaying oscillation which may be a clue.
I have tried many things in software and hardware, but cannot eliminate the noise.