I am working on LCD patterns through MSP430. According to the following website, when I set the registers starting from 0x40 to 0x48 and placing "Bell" pattern I will see a Bell on the display.
However, my program is showing something else! Meaning that I am not able to map the display in details. In other words, Only one charcter by character not pixle by pixle!
How I can do this?
The LCD is 8x2 and as I set LCD_command to 0x80 I can choose the leftmost top cell.
I am confused between CG address and DD address.
http://www.8051projects.net/lcd-interfacing/lcd-custom-character.php
- void LCD_build(unsigned char location, unsigned char *ptr){
- unsigned char i;
- if(location<8){
- LCD_command(0x40+(location*8));
- for(i=0;i<8;i++)
- LCD_senddata(ptr[ i ]);
- }
- }
or
LCD_cmd(0x40); //Load the location where we want to store // CG RAM Address
LCD_dat(0x04); //Load row 1 data *** make a Bell shape!
LCD_cmd(0x41);
LCD_dat(0x0E); //Load row 2 data
LCD_cmd(0x42);
LCD_dat(0x0E); //Load row 3 data
LCD_cmd(0x43);
LCD_dat(0x0E); //Load row 4 data
LCD_cmd(0x44);
LCD_dat(0x1F); //Load row 5 data
LCD_cmd(0x45);
LCD_dat(0x00); //Load row 6 data
LCD_cmd(0x46);
LCD_dat(0x04); //Load row 7 data
LCD_cmd(0x47);
LCD_dat(0x00); //Load row 8 data
But I cannot reach the single pixles! :(
Actually I do not understand the data-sheet of LCD 17 and 20!
Can anyone explain to me please?