I have two questions on MSP430F5232's power design.
- For MSP430F5232, all three powers VCC/AVcc/DVcc are tied together with two capacitors of 10uF and 0.1uF according to the reference design in the user manual (p.21/153 of SLAU278p). Is it a recommended power circuit design?
- I want to estimate the maximum power of the MSP430F5232. According to the table on page 46/104 of "SLAS897-Sept 2013", power can be estimated depending on its frequency when the Vcc is 3.0V. By the way, I am planning to use 3.3V of Vcc. In that case, is there a way of estimating its maximum power? Or is the power going to be very similar to the values shown in the table?