Hi.
I have ordered and received MSP-TS430RGC64C & MSP-FET430UIF along with MSP430F5229 uC.
After installing CCS Version:5.5.0.00077, I connected MSP-TS430RGC64C to the USB port through MSP-FET430UIF.
Then, I could see the famous “MSP430: Error connecting to the target: Unknown device” error.
According to several threads regarding this issue, the problem seems to be a hardware/connection issue.
By the way, there was the following note which came with the product.
************************
Important: For correct JTAG connection, programming, and debug operation, it is important to follow this
procedure:
1. Make sure that the VCC and DVIO voltage supplies are OFF and that the power rails are fully
discharged to 0 V.
2. Enable the 1.8-V external DVIO power supply.
3. Enable the 1.8-V to 3.6-V VCC power supply (alternatively, this supply can be provided from the MSPFET430UIF
JTAG debugger interface).
4. Connect the MSP-FET430UIF JTAG connector to the target board.
5. Start the debug session using IAR or CCS IDE.
*********************************************
The user-guide also says that "This development platform does not supply the 1.8-V DVIO rail on board and it MUST be provided by external power supply for proper device operation".
So, does "step 2" mean that “I need to provide 1.8V from an additional power supply through additional power cable”?
Thank you.