I am using
- MSP430F47186
- IAR EW for MSP430
In the memory information after compiling code, I obtain from IAR EW like
CODE : 34 840
DATA: 6 767
CONST: 2 100
In IAR EW document (EW430_CompilerReference.pdf), the explanation of these memory segments is
-----
CODE - for executable code
DATA - for data placed in RAM
CONST - for data placed in ROM
-----
I would like to know the maximum size for CONST (ROM) memory for MSP430F47186.
In msp430F47186.pdf, page 16, I found "memory organization".
In this Table (memory organization), which parts corresponds to "CONST" memory type?
Does the 1st category in the table (i.e. "Memory > Main: code memory | Flash") includes both
- Code
- CONST memory segment
in the one memory segment?