We have a working design using the MSP430G2230, that we now wish to modify to use the 2210 (for the internal analog comparator). Using the IAR toolchain, and removing the code that relates to differences, I can compile and download to the 2230 and the code runs correctly. When I download to the 2210, the reset vector is unprogrammed and therefore the part goes into its "low power, unprogrammed, on-the-shelf stock" mode of conserving power. I can select either 2230 or 2210 as the build target, and I get the appropriate warning when downloading into the opposite processor. But either target selected, when I download to the 2210, I get a blank reset vector. Surely I'm just missing a setting somewhere in the IAR tools, but I can't find it.